Xiao Nrf52840 sense - which BSP?

The HX711 breakout is connected through 2gpios (data,clock).
Imu read angular velocity 80 times/sec.
The system is already working with a xiao Esp32c3 on a custom board, but the power consumption is too high, even in deep sleep. Also I have some issue at the first power up after the battery discharge, always I need to hardreset the board, which is not an option.
For these reasons I’m switching to the Nrf52840

1 Like