XIAO nRF52840 Sense bricked. Reset not working,

Hi,
I somehow was able to brick my board (probabaly by writing to the flash).
Reset by double-tapping the reset switch is not doing anything :-/
What can I do? any ideas?
Ran

Does it have the LED on? Can the device be seen in the device manager?

Hi, Citric - no to both questions.

This may be the last method. Please refer to it.

That requires speacial hardware, right? Any way around that?

Sorry, as far as I know there is no other way for now.

I was also struggling with this and thought the board was toast. The solution was to:
in arduino IDE, go to preferences>>“show verbose output during (upload=true)”
Then upload your sketch. You will see the console trying all of the available ports, when you see it doing this double tap the reset button as fast as possible. The delay between taps has to be very fast.

When the bootloader is lost, the only way to restore it is using the JTAG interface. The lowest cost Segger JTAG is the Jlink EDU mini for about 15 USD, or the JLINK Edu for about 50 USD. You may also consider getting the seeed XIAO expansion base, since it simplifies access to the JTAG pads.
This is as well a useful investment, since it allows to so hardware source code debugging at the board with all the nice features as single step, breakpoints, data inspection, etc.

My XIAO nRF52840 BLE Sense Reset button has gone, is there any option to reset and get into the boot mode

Hi there,
yes, Those Tiny little nubs of a button , come off if you get a little Too Much fingernail action on the reset button. The only other way AFAIK , is the expansion base has a reset button that works for one I have with the same handicap.
HTH
GL :slight_smile: PJ

if the expansion base works then he should be able to manually short the pad

i think you pull the pin to ground

this is for SAMD but i think the procedure is the same

single click for reset and double click for bootloader

Enter Bootloader Mode ​

Sometimes the Seeed Studio XIAO SAMD21 port may disappear when user programming process fails. we can solve this problem by the following operation:

  • Connect the Seeed Studio XIAO SAMD21 to your computer.
  • Use tweezers or short lines to short the RST pins in the diagram twice.
  • The orange LED lights flicker on and light up.

At this point, the chip enters Bootloader mode and the burn port appears again. Because the samd21 chip has two partitions, one is the Bootloader and the other is the user program. The product will burn a bootloader code in the system memory when it leaves the factory. We can switch modes by performing the above steps.

Yes. :grinning: :+1:
Expansion board does that exactly…
GL :slight_smile: PJ

Hi PJ_glasso! would you mind to help me with this problem? if i press the rst button twice, usually the driver XIAO will shows in my driver manager, but somehow after i flash some ble mesh program (the zephyr.uf2 file) from nrf connect example i did not get anything from it. After that, when i tried to press twice the rst button, the driver XIAO didn’t show up and my nRF52840’s port won’t recognize in my laptop. Can you tell me why and how to solve it?

Hi there,

Yes, So sometimes the code can overwrite the “BootLoader” firmware and that’s why it appears bricked. Try first HOLD the RESET button WHILE you PLUG in the USB port,(it’s tricky but doable) that may recover it and then send a blinky sketch or drag and drop a RGB Blink example uF2 file fromt he Drag & Drop Testing thread(search) if those don’t recover it You may need to do the unbrick procedure on the WiKi.

HTH
GL :slight_smile: PJ :v:

Congratulations on getting to level 2 of the Xiao skill set… Everyone does it one time or another so Not a big deal. :+1: great learning opportunity