🤠 Xiao Expansion board drag & drop testing uf2 flash files

Here is a almost full Monty,
Adds SD test, RTC, and some BLE LED control rolled in. :wink: :+1:
if you have a Mobile or Nrf connect for Desktop with a Nordic Dongle , Another $9 tool a must have.


Enjoy , Drag & Drop.
SelfTest_Xiao_Expansion.zip (264.3 KB)

This is the Serial output


Power ON 
 
Xiao Expansion board and MCU check & Test compiled on Mar 23 2024 at 17:42:35
Processor came out of reset.

Selected MCU: nRF52840

Xiao Unit: EA52
Playing startup sound
RTC Date & Time is:3/19/24 10:17:21
Testing R G B LED - RED, GREEN, BLUE... 

Initializing SD card...Card Mounted
Card type: SDHC
Volume type is:    FAT32
SD Volume size (Gb):  29.12

Xiao MAC: BF:49:C1:6B:01:4D

Advertising Bluetooth Device
  as: Xiao EA52
Connected to central: c8:65:29:7e:60:0c // this will pop in when you connect to it.

HTH
GL :slight_smile: PJ :v:

3 Likes