Xiao esp32s3 wio-sx1262 Lora Kit as P2P LoRa node

Hi there,

So My set is in transit… But which BSP are you using to compile with? Have you tried the older ones?
You are very close :sweat_smile:, Looks like the INIt for Lora is failing? (mr obvious)
do you have any other LORA stuff? Grove Lora board maybe?

I think it needs a string or command with a CRC or something, is it communicating with the SX or NO?
Keep going maybe someone else can comment, but try rolling back the BSP and see if it improves? :+1:

HTH
GL :slight_smile: PJ :v:

I’m grabbing a set of these new boards too.


The Wi-Fi Halow Board based on the FGH100M-H module is a high-performance, long-range Wi-Fi HaLow solution. Operating in the 902-928 MHz frequency band, it offers excellent penetration and coverage, making it ideal for smart home and IoT applications. With its compact design and compatibility with the Seeed Studio XIAO ecosystem, this card ensures reliable and efficient connectivity for various projects.

1 Like