Xiao esp32s3 wio-sx1262 Lora Kit as P2P LoRa node

After scouring the internet for information i found several suggestions as to what the pins are through the b2b connector but still not getting anywhere, updated sketch below and some information links I’ve gathered:

This one i suspect should be most reliable:

#include <SPI.h>
#include <RadioLib.h>
#include <OneWire.h>
#include <DallasTemperature.h>

// ✅ Updated Pin Configuration (B2B Connector)
#define LORA_NSS 41    // ✅ SPI Chip Select (GPIO41)
#define LORA_SCK 7     // ✅ SPI Clock (GPIO7)
#define LORA_MOSI 9    // ✅ SPI MOSI (GPIO9)
#define LORA_MISO 8    // ✅ SPI MISO (GPIO8)
#define LORA_RST 42    // ✅ LoRa Reset (GPIO42)
#define LORA_BUSY 40   // ✅ LoRa BUSY (GPIO40)
#define LORA_DIO1 39   // ✅ LoRa IRQ (DIO1 - GPIO39)
#define LORA_ANT_SW 38 // ✅ Antenna Switch (GPIO38)

// ✅ Temperature Sensor Configuration
#define ONE_WIRE_PIN 2  // DS18B20 data pin
OneWire oneWire(ONE_WIRE_PIN);
DallasTemperature sensors(&oneWire);

// ✅ Battery Voltage Monitoring
#define BATTERY_PIN 4  // ADC pin for battery voltage

// ✅ LoRa Configuration
#define LORA_FREQUENCY 868E6  
#define LORA_SPREADING_FACTOR 12  
#define LORA_BANDWIDTH 125E3  
#define LORA_CODING_RATE 5  
#define LORA_TX_POWER 22    

// ✅ Ensure Device Starts the Transmission
#define INITIATING_NODE  

// ✅ LoRa Module Instance
Module mod(LORA_NSS, LORA_DIO1, LORA_RST, LORA_BUSY);
SX1262 radio(&mod);

void setup() {
    Serial.begin(115200);
    while (!Serial);
    Serial.println("[SX1262] LoRa Initialization - Correct B2B Pins");

    // ✅ Initialize SPI Bus with Correct Pins
    Serial.println("[SPI] Initializing...");
    SPI.begin(LORA_SCK, LORA_MISO, LORA_MOSI, LORA_NSS);
    Serial.println("[SPI] Initialized!");

    // ✅ Reset SX1262
    Serial.println("[SX1262] Resetting module...");
    pinMode(LORA_RST, OUTPUT);
    digitalWrite(LORA_RST, LOW);
    delay(10);
    digitalWrite(LORA_RST, HIGH);
    delay(10);
    Serial.println("[SX1262] Reset Complete!");

    // ✅ Initialize Temperature Sensor
    Serial.println("[TEMP] Initializing DS18B20...");
    sensors.begin();

    // ✅ Initialize LoRa
    Serial.println("[SX1262] Initializing LoRa...");
    SPI.beginTransaction(SPISettings(500000, MSBFIRST, SPI_MODE0)); // Reduce SPI Speed
    int state = radio.begin(LORA_FREQUENCY, LORA_BANDWIDTH, LORA_SPREADING_FACTOR, LORA_CODING_RATE, 
                            0x12, LORA_TX_POWER, 8, 1.6, false);
    SPI.endTransaction();

    Serial.print("LoRa Init Status: ");
    Serial.println(state);

    if (state == RADIOLIB_ERR_NONE) {
        Serial.println("✅ [SUCCESS] LoRa initialized successfully!");
    } else {
        Serial.println("❌ [ERROR] LoRa initialization failed!");
        Serial.print("🔎 [ERROR CODE] ");
        Serial.println(state);
        while (true) {  // Prevent further execution if LoRa fails
            delay(100);
        }
    }

    #ifdef INITIATING_NODE
        sendLoRaData();
    #else
        radio.startReceive();
    #endif
}

void loop() {
    delay(15000);
    Serial.println("[SX1262] Sending new LoRa data...");
    sendLoRaData();
}

// ✅ Read Temperature from DS18B20
float readTemperature() {
    Serial.println("[TEMP] Reading temperature...");
    sensors.requestTemperatures();
    float temp = sensors.getTempCByIndex(0);
    Serial.print("[TEMP] Temperature: ");
    Serial.print(temp);
    Serial.println(" °C");
    return temp;
}

// ✅ Read Battery Voltage using 220KΩ / 100KΩ Voltage Divider (16-sample averaging)
int readBatteryVoltage() {
    long sum = 0;
    for (int i = 0; i < 16; i++) {
        sum += analogReadMilliVolts(BATTERY_PIN);
        delay(5);
    }
    float measuredMilliVolts = sum / 16.0;
    int batteryMilliVolts = measuredMilliVolts * 3.2; // Voltage divider correction
    Serial.print("[BATTERY] Voltage: ");
    Serial.print(batteryMilliVolts);
    Serial.println(" mV");
    return batteryMilliVolts;
}

// ✅ Convert Battery Voltage to Percentage
int getBatteryPercentage(int batteryMilliVolts) {
    int fullCharge = 4200;  // Fully charged at 4.2V
    int emptyCharge = 3200; // Minimum voltage before shutdown at 3.2V
    int batteryPercentage = ((batteryMilliVolts - emptyCharge) * 100) / (fullCharge - emptyCharge);
    return constrain(batteryPercentage, 0, 100);
}

// ✅ Read RSSI (Signal Strength)
int readRSSI() {
    return radio.getRSSI();
}

// ✅ Send Data Over LoRa
void sendLoRaData() {
    float temperature = readTemperature();
    int batteryMilliVolts = readBatteryVoltage();
    int batteryPercentage = getBatteryPercentage(batteryMilliVolts);
    int rssi = readRSSI();

    // ✅ Construct JSON message
    char message[128];
    snprintf(message, sizeof(message),
             "{\"hostname\":\"ESP32S3\", \"temp\":%.2f, \"batt\":%d, \"rssi\":%d}",
             temperature, batteryPercentage, rssi);

    Serial.print("[SX1262] Sending packet: ");
    Serial.println(message);

    int transmissionState = radio.startTransmit(message);
    if (transmissionState == RADIOLIB_ERR_NONE) {
        Serial.println("✅ [SUCCESS] Transmission Complete!");
    } else {
        Serial.print("❌ [ERROR] Transmission Failed, Code: ");
        Serial.println(transmissionState);
    }
}

Current Result:

15:04:25.649 -> [SX1262] LoRa Initialization - Correct B2B Pins
15:04:25.649 -> [SPI] Initializing...
15:04:25.649 -> [SPI] Initialized!
15:04:25.649 -> [SX1262] Resetting module...
15:04:25.753 -> [SX1262] Reset Complete!
15:04:25.753 -> [TEMP] Initializing DS18B20...
15:04:25.772 -> [SX1262] Initializing LoRa...

Sits like that indefinitely, away to do something else and come back to it with a clear head.

2 Likes