XIAO ESP32S3 & Wio-SX1262 Kit for Meshtastic & LoRa

Hello –

As I see you have the kit mounted upon a Xiao Expansion Board, I wonder what you have found with the PIN_BUTTON at 1 and the PIN_BUZZER at 3?

When I attempt to set those pins in the app, Radio Config>Device Config> and attempt redefine those pins, I get no-joy. In fact I lose function of the USER BUTTON on the Wio board, for like scrolling screens. I carousel 5" because I don’t like mashing that button (board) through to the B2B connxn. Anyway, the Wio button maps to GPIO21 and maybe there is a way to do something with that.

Anyway the Wio board takes up the 1 and 3 pins with its BUSY and NSS (SPI_CS?) pins. So wondering what experience you have in these matters?

Thanks