Hi, Is there not a USER LED under the boot button:
Also I am worried about why the WIO-E5 can not be detected
Sketch uses 314593 bytes (9%) of program storage space. Maximum is 3342336 bytes.
Global variables use 19568 bytes (5%) of dynamic memory, leaving 308112 bytes for local variables. Maximum is 327680 bytes.
esptool.py v4.5.1
Serial port /dev/cu.usbmodem1101
Connecting...
Chip is ESP32-S3 (revision v0.2)
Features: WiFi, BLE
Crystal is 40MHz
MAC: 74:4d:bd:81:b4:40
Uploading stub...
Running stub...
Stub running...
Changing baud rate to 921600
Changed.
Configuring flash size...
Flash will be erased from 0x00000000 to 0x00003fff...
Flash will be erased from 0x00008000 to 0x00008fff...
Flash will be erased from 0x0000e000 to 0x0000ffff...
Flash will be erased from 0x00010000 to 0x0005cfff...
Compressed 15104 bytes to 10399...
Writing at 0x00000000... (100 %)
Wrote 15104 bytes (10399 compressed) at 0x00000000 in 0.3 seconds (effective 459.4 kbit/s)...
Hash of data verified.
Compressed 3072 bytes to 146...
Writing at 0x00008000... (100 %)
Wrote 3072 bytes (146 compressed) at 0x00008000 in 0.1 seconds (effective 384.2 kbit/s)...
Hash of data verified.
Compressed 8192 bytes to 47...
Writing at 0x0000e000... (100 %)
Wrote 8192 bytes (47 compressed) at 0x0000e000 in 0.1 seconds (effective 601.3 kbit/s)...
Hash of data verified.
Compressed 314960 bytes to 179936...
Writing at 0x00010000... (9 %)
Writing at 0x0001b5e9... (18 %)
Writing at 0x00024773... (27 %)
Writing at 0x0002a0b0... (36 %)
Writing at 0x0002f78a... (45 %)
Writing at 0x00034b1a... (54 %)
Writing at 0x0003a31e... (63 %)
Writing at 0x00042fd8... (72 %)
Writing at 0x0004b573... (81 %)
Writing at 0x00051a0a... (90 %)
Writing at 0x000570cb... (100 %)
Wrote 314960 bytes (179936 compressed) at 0x00010000 in 2.6 seconds (effective 961.0 kbit/s)...
Hash of data verified.
Leaving...
Hard resetting via RTS pin...