Hi there,
And Welcome here, Just reply or comment on this thread or another that is close to build some forum cred, then you can do everything.
It’s a spammer control/prevention… they got hit a while back so it may not be updated in the FAQ, ![]()
Which Board support package file are you compiling with?
also if using Arduino IDE be sure ArduinoBLE is NOT an installed LIB on the system.
HTH
GL
PJ ![]()
I have a example I’ll be posting that uses the S3 with 3 Concurrent BLE connections and 6 Notifies… all working, and the Round Display. so Stay tuned. ![]()
Take a look at this code here
🧐 Round Display w/TouchRing BLE Xiao C6 & S3-Plus - #2 by PJ_Glasso
It may be the BSP you are using, check that roll it back one and go again
![]()