I was trying to get the HardwareTest app for the Seeed Round Display running on my XIAO ESP32C3 and have run into a problem:
ELF file SHA256: 27130e8b14f58bba
11:11:15.012 ->
11:11:15.012 -> Rebooting...
11:11:15.012 -> ESP-ROM:esp32c3-api1-20210207
11:11:15.012 -> Build:Feb 7 2021
11:11:15.012 -> rst:0x3 (RTC_SW_SYS_RST),boot:0x9 (SPI_FAST_FLASH_BOOT)
11:11:15.012 -> Saved PC:0x40381cc8
11:11:15.012 -> SPIWP:0xee
11:11:15.012 -> mode:DIO, clock div:1
11:11:15.012 -> load:0x3fcd5810,len:0x438
11:11:15.044 -> load:0x403cc710,len:0x90c
11:11:15.044 -> load:0x403ce710,len:0x2624
11:11:15.044 -> entry 0x403cc710
11:11:15.143 -> XIAO round screen - LVGL_Arduino
11:11:15.143 -> Guru Meditation Error: Core 0 panic'ed (Store access fault). Exception was unhandled.
11:11:15.143 ->
11:11:15.143 -> Core 0 register dump:
11:11:15.143 -> MEPC : 0x4202bd74 RA : 0x4202bd66 SP : 0x3fca3510 GP : 0x3fc8c200
11:11:15.143 -> TP : 0x3fc8f850 T0 : 0xffffffff T1 : 0xffc3ffff T2 : 0x00000001
11:11:15.143 -> S0/FP : 0x60004000 S1 : 0x3fc8eb4c A0 : 0x00000001 A1 : 0xffffffff
11:11:15.175 -> A2 : 0x00000000 A3 : 0xfdffffff A4 : 0x08000000 A5 : 0x00000010
11:11:15.175 -> A6 : 0x00000000 A7 : 0x04c4b400 S2 : 0x00000001 S3 : 0x00000000
11:11:15.175 -> S4 : 0x00000000 S5 : 0x00000000 S6 : 0x00000000 S7 : 0x00000000
11:11:15.175 -> S8 : 0x00000000 S9 : 0x00000000 S10 : 0x00000000 S11 : 0x00000000
11:11:15.207 -> T3 : 0x00000000 T4 : 0x0000000f T5 : 0x003c0000 T6 : 0x00000003
11:11:15.207 -> MSTATUS : 0x00001881 MTVEC : 0x40380001 MCAUSE : 0x00000007 MTVAL : 0x00000010
11:11:15.207 -> MHARTID : 0x00000000
11:11:15.207 ->
11:11:15.207 -> Stack memory:
Which would normally mean just re-flashing and going on, or, at worst, erasing the flash and starting over.
But that’s the problem. With this running, I can’t erase the flash.
% /Users/davidgs/Library/Arduino15/packages/esp32/tools/esptool_py/4.5.1/esptool --chip esp32c3 --port /dev/cu.usbmodem83201 erase_flash
esptool.py v4.5.1
Serial port /dev/cu.usbmodem83201
Connecting...
Chip is ESP32-C3 (revision v0.4)
Features: WiFi, BLE
Crystal is 40MHz
MAC: 64:e8:33:8b:87:8c
Uploading stub...
Running stub...
Stub running...
A fatal error occurred: Unable to verify flash chip connection (No serial data received.).
I’ve tried unplugging it, holding down the boot button and plugging it back in, etc. Nothing seems to help.
How can I recover this device?