Hello,
I am controlling a motor using MCPWM with a xiao ESP32-S3 Sense, but this stops working if I call SD.begin().
Any known conflict between MCPWM and SD card reader ?
Thanks,
Hello,
I am controlling a motor using MCPWM with a xiao ESP32-S3 Sense, but this stops working if I call SD.begin().
Any known conflict between MCPWM and SD card reader ?
Thanks,
Hi there,
If you set the default Settings (GPIO’s) the PWM conflicts with the SD CS.
Afaik , you need to Switch it in the code or hardware or both?
without seeing the Hardware connections and the code in question it’s merely a Guess.
HTH
GL
PJ
check out the technical reference guide about IO mux and GPIO matrix to see the way .
![]()
try calling SDbegin() with a different PIN explicitly see if it works?
Hello PJ, and thanks for the insight.
I was trying to use GPIO7 (D8/SCK) & GPIO8 (D9/MISO) for my motor, and indeed SD.begin(21) does interfere with these pins, not with MCPWM per se.
It seems I misread the schematic, thinking that SD Card was using dedicated SPICLK and SPID pins… but Iooking at the File System documentation, I now understand SD operation does use D8/D9/D10.
Sorry for missing the obvious.
N.B. I found MCPWM rather useful to avoid using the limited number of PWM channels on ESP32S3… I’ve packaged a little library to make it easy to use.
Hi there,
I agree with you, way more useful too. Simple thing easy fix
![]()
Too many variants
LOL, c2,c3,why no C4 ,
I guess it just sounds bad …
GL
PJ
![]()