XIAO ESP32-C3 won't boot when powered from 5V pin

I have a BLE program that runs flawlessly when my XIAO ESP32-C3 module is plugged into my computer via USB-C. However, whenever my module is powered with 4.96 VDC through the 5V pin, no code is executed. The CH light turns on and I measure exactly 4.96 VDC on the 5V pin, and 3.34 VDC on the 3.3V pin. If I plug the module into my computer at any point, it will start working, and when I unplug it, it immediately stops working, even if the external supply is present.

I added a 47 uF (50V) capacitor directly between the 5V pin and the GND pin next to it, and a 10 uF (50V) capacitor directly between the 3.3V pin and GND. Neither had any effect on the circuit.

The 5V (or rather, 4.96 VDC) supply is a buck regulator and the level is quite stable. Holding down the RST pin for a bit after the buck regulator powers up doesn’t help.

There are NO while (!Serial) or similar statements in my code.

I’ve seem a few people with similar problems but no one has figured out why these modules don’t like being powered externally. Any ideas?

Best,
Nick

contrary to popular belief… i do not think you can power thru the 5v pin… it is a one way power out not power in… people on here will disagree with me… but hey… whatever… try powering thru the bottom battery pads

Thanks for the reply. I don’t have a supply lower than 5 VDC around right now but I will set something up tonight and update here.

these devices have onboard battery management chips… i assume they provide regulated 3v3 at that pin and not the 5v pin… you may try powering via USB power bank… but i am thinking the bottom line is you cant power thru the 5V pin… even though some documentaton says you can

Hi nblanch,
Experiment with a thorough understanding of the schematic and component data sheets.
The following two connections are risky.

  1. simultaneously supplying 5V from USB and 5V from the 5V pin
  2. connecting a power source other than the battery to the battery pad.

nblanch,

Can you please be more specific?
Would a simple “Blink” sketch without serial.print change the situation?

Appreciate the links. It’s a strange situation… based on the schematics, it appears that the VUSB pin is the 5V pin that is broken out. There is nothing preventing our external 5V supply from generating the 3.3V required for the chip. In fact, if we measure 3.3V on the broken out 3.3V pin (which I do), then it indicates the chip should be receiving 3.3V, because the broken out 3.3V pin is on the same net as the 3.3V supply directly to the chip.

When I said ‘immediately stops working’, I mean all code execution stops and the BLE activity ceases.

With a simple blink sketch, the Xiao does not execute code immediately on startup. However, if I hold down the reset button for ~1 second after the 5V supply stabilizes, then it is able to successfully execute the blink routine while being powered through the 5V pin. The failure on initial power-up is probably due to a slow rise time of the switching regulator and/or the charge time for the large decoupling caps, which is more or less expected behavior in this case and not the fault of the Xiao.

C3 has a peak current flow of about 60-70mA when BLE is activated. Can an external 5V supply this peak current?

I am using an AP63205 2A regulator https://www.diodes.com/assets/Datasheets/AP63200-AP63201-AP63203-AP63205.pdf. However, the 12 VDC source that I am stepping down to 5 VDC is only rated for 800 mA max. I thought that 800 mA @ 12 VDC would be enough (and it should be), but there’s a chance that a large inrush current upon starting up the Xiao drops the voltage enough (loading effect) to cause an issue.

I don’t see any specific numbers for ESP32-C3 current spikes upon power-up, but some people have measured in the 200s of mAs during BLE advertising. Investigating ESP32-C3 Power Management | robdobson.com

So, I switched to a much larger 12 VDC supply with a 6A max and my program now seems to be executing, with Serial.print() and all. BLE works as intended.

This was certainly not the Xiao’s fault. There must have been some transients on the power line that require an oscilloscope to notice. For anyone else having trouble powering via 5V pin, try using an oversized power supply, even if you’re already using one that should theoretically work and the 5 VDC and 3.3 VDC values look totally fine. Alternatively, powering from a battery would avoid this situation in the first place.

Thanks for the help troubleshooting!