XIAO esp32 C3 is showing this error on Arduino IDE while uplaoding code

Arduino: 1.8.19 (Windows 10), Board: “XIAO_ESP32C3, Enabled, Default 4MB with spiffs (1.2MB APP/1.5MB SPIFFS), 160MHz (WiFi), QIO, 80MHz, 4MB (32Mb), 115200, None, Disabled”

Sketch uses 806044 bytes (61%) of program storage space. Maximum is 1310720 bytes.

Global variables use 35612 bytes (10%) of dynamic memory, leaving 292068 bytes for local variables. Maximum is 327680 bytes.

esptool.py v4.2.1

Serial port COM10

Connecting…Traceback (most recent call last):

File “esptool.py”, line 34, in

Chip is ESP32-C3 (revision 4)

File “esptool_init_.py”, line 1004, in _main

Features: Wi-Fi

File “esptool_init_.py”, line 790, in main

Crystal is 40MHz

File “esptool\loader.py”, line 1108, in flash_set_parameters

MAC: 34:85:18:00:8d:b8

File “esptool\loader.py”, line 406, in check_command

Uploading stub…

File “esptool\loader.py”, line 375, in command

Running stub…

File “esptool\loader.py”, line 307, in read

Stub running…

StopIteration

Configuring flash size…

[11328] Failed to execute script ‘esptool’ due to unhandled exception!

An error occurred while uploading the sketch

This report would have more information with
“Show verbose output during compilation”
option enabled in File → Preferences.

Hi there,
Can you use the </>tags and paste the code in there, It will make it easier for us to help,
Thanks. Which BSP are you using, Try to roll back.
If you enable the verbose output on the settings, The compiler output will tell You and US more.
Post the first 4 lines and the last 12 b4 the upload begins or Fails.
HTH
GL :slight_smile: PJ

You can enter bootloader mode to solve the problem that XIAO ESP32C3 can’t be uploaded

Thanks. This solved my issue without requiring MORE information.