XIAO_BLE wakes up from System_ON_Sleep and Writes weather data to on-board Flash

The value of PowerDownTime when release is possible is not stable at all. However, if it is short, it can be released, and if it is long, it cannot be released. Somehow, it seems to be related to Serial.print().
I have ordered an external Flash so that the signal can be observed on a digital oscilloscope.
This is going to be a long term project.