Hello,
Is this thing ON? Why is it marked SOLVED? WTH? ![]()
I wonder if we will ever be able to read the battery voltage on the Xiao nRf52840 BLE Sense micro?. Why is this a problem? I’m using
Using library ArduinoBLE at version 1.3.4 in folder: D:\Arduino_projects\libraries\ArduinoBLE
Using library Seeed Arduino LSM6DS3 at version 2.0.3 in folder: D:\Arduino_projects\libraries\Seeed_Arduino_LSM6DS3
Using library Wire in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\Seeeduino\hardware\mbed\2.9.1\libraries\Wire (legacy)
Using library SPI in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\Seeeduino\hardware\mbed\2.9.1\libraries\SPI (legacy)
--Removed for clarity--
Sketch uses 342496 bytes (42%) of program storage space. Maximum is 811008 bytes.
Global variables use 72160 bytes (30%) of dynamic memory, leaving 165408 bytes for local variables. Maximum is 237568 bytes.
Everything else works, C’mon Seeed what’s up with this stuff?
GL
![]()