Xiao BLE Sense compilation error

Hello

I have troubleshooting when i compile.
“C:\Users\Thierry\AppData\Local\Arduino15\packages\Seeeduino\hardware\mbed\2.9.1\cores\arduino/mbed/platform/include/platform/Callback.h:20:10: fatal error: cstring: No such file or directory”

I’m using Arduino IDE 2.0.3 under windows 10.


false, true, bool, FALLING and INPUT_PULLUP are also unknown, may be some others…

Thanks a lot for your help.
Best Regards

Hi, I would try to uninstall it from the boards tab, and then install the 2.9.0 and It fixed some weird errors I was getting and Interrupts not working right .
HTH
LML
GL :slight_smile:

I will try it
Thanks