When using “Seeed nRF52 Boards 1.0.0”,
#include <Arduino.h>
#include <Adafruit_TinyUSB.h>
may be required.
Please also refer to the following
It may not be the right way, but I am using the IMU implemented in “Seeed XIAO nRF52840 Sense” on “Seeed nRF52 Borads 1.0.0” (non mbed) in the following way
Board library: Seeed nRF52 Borads 1.0.0 (non mbed)
Board : Seeed nRF52 Borads / Seeed XIAO nRF52840 Sense
IMU library: Seeed_Arduino_LSM6DS3
–>Replace “Wire” in LSM6DS3.cpp with “Wire1”.
“#define Wire Wire1” does not work as expected, so I rewrote Wire to Wire1.
Or if you use “Seeed nRF52 mbed-enabled Boards 2.8.1”, IMU will work without any problem.