XIAO Awesome Product Lineup- Must Haves

XIAO Awesome Product Lineup- Must Haves

These are a list of all the important XIAO related products that are must have… IMO

Seeed Studio Expansion Board Base for XIAO

Seeed Studio Grove Base for XIAO

L76K GNSS Module for Seeed Studio XIAO

Round Display for Seeed Studio XIAO

Seeed Studio XIAO ESP32-S3 Sense

XIAO nRF52840 & Wio-SX1262 Kit for Meshtastic

XIAO ESP32S3 & Wio-SX1262 Kit for Meshtastic & LoRa

CAN Bus Breakout Board for Seeed Studio XIAO

RS485 Breakout Board for Seeed Studio XIAO

COB LED Driver Board for Seeed Studio XIAO

LED Driver Board for Seeed Studio XIAO

Bus Servo Driver Board for Seeed Studio XIAO

1-Channel Relay for Seeed Studio XIAO

XIAO Logger HAT

6x10 RGB WS2812 Matrix for Seeed Studio XIAO

XIAO PowerBread

Aluminum Heat Sink for Seeed Studio XIAO

7-Pin Male Header for Seeed Studio XIAO

2.4GHz Rod Antenna (2.81dBi) for Seeed Studio XIAO

Grove - 4 pin Female Jumper to Grove 4 pin Conversion Cable

Grove - UART Crossover Cable 4Pin 20cm

Hey, great collection is shown here. it’s wild how much tech they’ve squeezed into a footprint no bigger than a postage stamp. It’s definitely my go-to when I’m tired of bulky boards and just want something sleek and powerful for a wearable or a tiny sensor.
Maybe I use many of them in my projects soon.

Thank you. Can you suggest only 1/2 products for those who never worked with XIAO before, but wishes to give a start?

lol… yes

I got carried away… its hard to choose.. because I do not know what your prefered use is… but

If you have never worked with Grove Sensors before, I would recomend starting with this product.

Technically this is not even XIAO level yet… This product has the sensors you will need and an arduino compatable board.. which is almost as good as a XIAO. With this product alone.. you can learn the basics

Now if you wish to move ahead to XIAO

Minimum Required

Select your flavor of XIAO, at a minimum

Seeed Studio XIAO SAMD21 (Pre-Soldered) - Seeeduino XIAO

Seeed Studio Grove Base for XIAO

Then consider adding

Seeed Studio Expansion Board Base for XIAO

I ordered the LoRa module for Xiao, waiting for it to ship right now

Welcome!

Cant wait for you to level up to the max!