i buy 5 components last week :
-1 Arduino Uno R3
-Xbees Dual Shield http://www.seeedstudio.com/depot/bees-shield-p-672.html?cPath=132_134
-2 RF Module Xbee Serie 2
-1 USB Explorer for Xbee (seedstudio).
I install all drivers for all.
I install X-CTU software from digi.com
When i plug each module on USB explorer and make Test/Query in X-CTU, all works good.
Each Module have same config.
But when i try Test/Query each module from Xbees Dual Shield, nothing works.
I place the Xbee RF Module on Xbee1 slot, switch to Amega, and run a Test/Query.
here is a 2 screenshot of my result :
X-CTU ask me to Reset Xbee Shield for connect but when i press reset on Xbee shield, nothing happen .
After cancel, there is what’s appear :
Unable to communicate with modem.
note then my pin is set like this :
Anyone have a clue what is not work here for this example?
Thanks to share if you know something
Your french nooby
deray
October 8, 2012, 3:12am
2
Hi
You can’t directly configure your Xbee via Xbee1 slot of Bee Shield , it is connect to software serial port which jumper pin you set. But it will be enabled if you used Xbee2 slot when switch to USB . For more details and the connections, suggest you refer to the schematic.
Regards,
Deray
i set the baud rate of my bluetooth bee via usb explorer like this :
+STBD=9600
i close my sscom32E.exe and re open at 9600 but i get this :
Kk‚KëcJBkãKJkBKjcJBkcJcÿkÃkBÿkÃkBºò¾ü
if i try again at 38400 i get :
øxàxø€xàxà€€ø€øø€øø€øxàøøxàxø€€€øøxàxø€€€øøxàxø€€€ø€øø€€xøø€øxàxø€€€ø€øøøxàxø€xàxà€€øøxàxø€xàxà€€ø€øø€€xøø€øxàxø€xàxà€€ø€øø€€x
no possibility for me to put a blank space like usualy…
no more +BTSTATE:X
How i can restore the baud rate to 38400? ('Iam thinking first its be compatible 9600?).
i see in wiki : Command to change baud rate is persistent even after reset. Hence remember the baud rate for next use.
i reset ((manually’’ and UNO +xbee shield reset too but nothing.
How restore 38400 to BT Bee when is messed like this?
Thanks.
thank you for your article,My problem has been resolved.