Xadow, Vibration Motor, why is there no xadow topic

Hello @all,

i started with the Xadow and my goal is to control two vibration motor seperate from each other.
I followed the instructions http://www.seeedstudio.com/wiki/Xadow_-_Vibrator_Motor this works fine for one motor.
But my question is how to connect/control the second motor?
My full setup are two vibration motors, a nfc reader and a bluetooth module. Is it possible to connect/use this setup?

Thanks + Greats,
M

If you use a Xadow main board as a controller, it’s hard to do so.