Hi.
I’m running the following code on Xadow:
void setup()
{
Serial.begin(9600);
while(!Serial.available());
Xadow.init();
delay(2000);
Serial.println("Init over");
}
void loop()
{
Serial.println(“Sleeping”);
delay(1000);
Xadow.pwrDown(4000); // sleep for 1000ms
Xadow.wakeUp(); // wake up
Serial.println(“Wake”);
delay(1000); // delay 500 ms
}
The problem is that on the output I have:
Init over
Sleeping
Wake
Sleeping
It looks like it runs one time and then it hangs…any ideas?
Thanks,