Hi all,
I have purchased Xadow GSM+BLE but I can’t find any batteries with the required JST-SH connector in my zone. My question is: if I connect a battery to the breakout pins 3 and 6, could I charge this battery through the 5V microUSB?
Thank you.
Hi all,
I have purchased Xadow GSM+BLE but I can’t find any batteries with the required JST-SH connector in my zone. My question is: if I connect a battery to the breakout pins 3 and 6, could I charge this battery through the 5V microUSB?
Thank you.
Yes, I am doing so… according to schema, pins are the same.
I am doing it so…
It should, vbat should be vbat - but for me, the 11-pin connector has fix 3.3V instead of the battery: is it like for everyone or just my module is wrong?
(now I can’t connect several battery cells parallellto the bus to add extra power - yes, I know the risk of parallell lipo cells)