Hello,
When I run the gps_test example I am getting the following output
GPS UTC:16-2-28 13:20:55
GPS status is V
GPS latitude is -:0.000000
GPS longitude is -:0.000000
GPS speed is 0.000000
GPS course is 0.000000
GPS position fix is 0
GPS sate used is 0
GPS altitude is 0.000000
GPS mode is A
GPS mode2 is 1
GPS UTC:16-2-28 13:20:56
GPS status is V
GPS latitude is -:0.000000
GPS longitude is -:0.000000
GPS speed is 0.000000
GPS course is 0.000000
GPS position fix is 0
GPS sate used is 0
GPS altitude is 0.000000
GPS mode is A
GPS mode2 is 1
can anyone please help?
Thanks