X86J4105800 Power adapter specifications

Can you tell me, what are the voltage/current/wattage specifications of the power adapters that ship with the X86J4105800? I am wanting to put together a 4 or 5 node kubernetes cluster with these but would like to find a solution so I do not have to plug in 5 power adapters into a power strip.

Thank you!

Hi @EnergySmithe, The package comes with a 12v 2A, 5.5 mm barrel jack adapter. you can also power the Odyssey with 12V DC Type-C input.