Hi
I am able to control the Pin 7 using the example in getting started.
The example uses pin 7 as 337 and works fine. (echo 337 > export)
What are the values for the other gpio pins. how to use pin 18 for example? (echo ??? > export)
Thanks much Kenny
@ansonhe97 Please help check it
Thanks for your reply.
I got it all is now working fine.
Some how I missed the the Linux GPIO list.
It must be my age I’m 82 years old.
Thanks again.
What processor is driving the 40 pin GPIO. ATSAMD21? Or Celeron processor via some electronics?
It is celeron processor
do you have a python example for this board to control the GPIO pins?
Just read and write to the file system.Simple Python statements
Question re: 40 pin GPIO.
When I pull the pin down is it High Impedance or Open Drain. My preference is Open Drain if possible
Thanks