Hi everybody, i got this error message when trying to debug :
STMicroelectronics ST-LINK GDB server. Version 7.4.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : C:\Users\Tiger\source\repos\LoRaWan-E5-Node\Projects\Applications\LoRaWAN\LoRaWAN_End_Node\STM32CubeIDE\Debug\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
COM frequency = 24000 kHz
Target connection mode: Attach
Target connection failed
COM frequency = 8000 kHz
Target connection mode: Attach
Target connection failed
COM frequency = 3300 kHz
Target connection mode: Attach
Target connection failed
COM frequency = 1000 kHz
Target connection mode: Attach
Target connection failed
COM frequency = 200 kHz
Target connection mode: Attach
Target connection failed
COM frequency = 50 kHz
Target connection mode: Attach
Target connection failed
COM frequency = 5 kHz
Target connection mode: Attach
Target connection failed
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
But i can program the device using STM32CubeProgrammer
My debug config in IDE :
WHAT DID I MISS ???