I have an RPI with a WM1302 USB module connected to the RPI’s USB port.
I am trying to get the station.conf file to be configured properly.
{
/* If slave-X.conf present this acts as default settings /
“SX1302_conf”: { / Actual channel plan is controlled by server /
“lorawan_public”: true, / is default /
“clksrc”: 0, / radio_0 provides clock to concentrator /
/ path to the SPI device, un-comment if not specified on the command line e.g., RADIODEV=/dev/spidev0.0 /
“device”: “usb:/dev/ttyACM0”,
/ freq/enable provided by LNS - only HW specific settings listed here /
“radio_0”: {
“type”: “SX1250”,
“rssi_offset”: -215.4,
“rssi_tcomp”: {“coeff_a”: 0, “coeff_b”: 0, “coeff_c”: 20.41, “coeff_d”: 2162.56, “coeff_e”: 0},
“tx_enable”: true,
“antenna_gain”: 0
},
“radio_1”: {
“type”: “SX1250”,
“rssi_offset”: -215.4,
“rssi_tcomp”: {“coeff_a”: 0, “coeff_b”: 0, “coeff_c”: 20.41, “coeff_d”: 2162.56, “coeff_e”: 0},
“tx_enable”: true,
“antenna_gain”: 0
}
/ chan_multiSF_X, chan_Lora_std, chan_FSK provided by LNS /
},
“station_conf”: {
“radio_init”: “device”,
“RADIO_INIT_WAIT”: “5s”,
“RX_POLL_INTV”: “10ms”,
“log_file”: “stderr”,
“log_level”: “DEBUG”, / XDEBUG,DEBUG,VERBOSE,INFO,NOTICE,WARNING,ERROR,CRITICAL */
“log_size”: 10000000,
“log_rotate”: 3,
“CUPS_RESYNC_INTV”: “10s”
}
}
What is the right setting of the “radio_init” ? with that value it does not connect to the cloud.
Does the ST chip on the WM1302 module need to be flashed to a FW that is compatible with Semtech’s Basics Station ?
If I set another value in the “radio_init” then the module connects to the cloud, however after a minute or two it disconnects and does not recover.