Has anyone been able to configure this board/card configuration with the sx1302_hal git repository? I cant seem to find a combinatino of pins that will get the radio to start successfuly
1 Like
Found this link. Replace the reser_lgw.sh script with this one and it seems to come to life.
1 Like
The documentation here is not accurate, and I could not get it to work. The instructions also do not match the pinouts mentioned on the diagrams. Sadly, the documentation is generally very poor and missing.
The only combination that I could get to work, when using the WM1302-US915+ Pi Hat + SX1302_HAL was the following:
SX1302_RESET_PIN=17 # SX1302 reset
SX1302_POWER_EN_PIN=18 # SX1302 power enable
Still testing, as not 100% sure this is correct, lora_pkt_fwd does work, and the radios do initialize.