WM1302 PI HAT no available GPS coordinates available yet

You have to verify the UART settings on the Raspberry Pi, ensuring the serial port is enables and the baud rate matches the GPS module’s settings. Testing with another GPS module can help determine if the problem lies with the WM1302 PI Hat or the Raspberry Pi setup. Updating drivers and software, as well as confirming compatibility between the devices is also recommended. Regards