WIZNET etherenet shield v1.1 06A12 Compatibility?

Recently I purchased a Seeedstudio WIZNET 5100 ethernet shield v1.1 06A12 and I am unable to successfully get it running with Arduino 1.0.1 IDE on Arduino Duemilanove. I having working arduinos configured with the ‘Original’ Arduino Ethernet Shield and they work fine. Am I dealing with an unforseen incompatibility?

Thanks for any input you can provide.

Hi , if your board is the version of 1.1 , you need modify something.

please open your libraries:

libraries–>Ethernet–>utility–>w5100.h

/*

  • Copyright © 2010 by Cristian Maglie [email protected]
  • This file is free software; you can redistribute it and/or modify
  • it under the terms of either the GNU General Public License version 2
  • or the GNU Lesser General Public License version 2.1, both as
  • published by the Free Software Foundation.
    */

#ifndef W5100_H_INCLUDED
#define W5100_H_INCLUDED

#include <avr/pgmspace.h>
#include <SPI.h>

//#define W5200 //please add "//"before this code.

#ifdef W5200
#define MAX_SOCK_NUM 8
#else
#define MAX_SOCK_NUM 4
#endif
…
…

Enjoy yourself.

Thanks I’ll give that a try…

Unfortunately that did not work… Any other thoughts? Anyone?

‘Recently I purchased a Seeedstudio WIZNET 5100 ethernet shield v1.1 06A12 and I am unable to successfully get it running with Arduino 1.0.1 IDE on Arduino Duemilanove. I having working arduinos configured with the ‘Original’ Arduino Ethernet Shield and they work fine. Am I dealing with an unforseen incompatibility?
Thanks for any input you can provide.’

Thanks

Hi,what errors you have got when compiling it.(pictures or codes)

i just bought this ethernet shield from radioshack and im testing it but when i try connecting to 192.169.1.177

it doesnt work.

why is it?

im using arduino uno R3
WIZNET etherenet shield v1 06A12

can you share the library for this Ethernet shield?

i feel like this thing doesnt work.

im about to go to radioshack to return this and get the original one from arduino

seeedstudios products sucks!!!

i will never buy seeedstudios products in my life!

Hi , you can download this attachment and have a try.
Ethernet.zip (57.7 KB)