wireless programming stalker v2.0

Hi
first post here and can’t find this in a faq.
I’m trying to setup wirless programming using a uartbee 4.0 and a seeeduino stalker v 2.0 and just can’t get it to work.
I have followed ladtada’s tutorial , ladyada.net/make/xbee/midibee.html and as bridged the solder pad on the uartbee between RTS and DI03 ( bottom of bard under usb connector), but still no go!

Can anyone one tell me what I’m missing ?

thanks
michael

Do you use XBee Series 1?
What is the Arduino error message?

Thanks
Albert

Hi sorry
for the slow reply, been away.
I’m using 2 Xbee series 1 modules that have been paired. I 've tested the pairing using a dat logging example & can at least receive data.

The errro message I get from the IDE (v22) is

Binary sketch size: 1042 bytes (of a 30720 byte maximum)
avrdude: stk500_getsync(): not in sync: resp=0x00
avrdude: stk500_disable(): protocol error, expect=0x14, resp=0x51