Wireless Charging Module 106990017

Hello Forum,

I recently purchased a Seeed Studio Wireless Charging Module 106990017.

Question #1: Do I need to do any diode OR’ing to manage the direction of the current flow?

Question #2: I plan to have my battery simultaneously connected to both my circuit and charging module all of the time. In other words, do I need to disconnect the battery from the rest of my circuit while the battery is charging.

Question #3: I am using this charging module to charge a 3.7V LiPo battery. Doe this charging module have the proper circuitry to limit the charge…I think that the charging is based upon current and not voltage. So while the charging module outputs 5V, this won’t overcharge a 3.7V LiPo battery???

TIA,
–Neal