Hi,
I received my Wio Terminal this morning
However I have hit a problem straight away.
My machine is Linux, Ubuntu 18.04
I installed Visual Studio Code, and the Seed ArduPy extention as advised. I have the terminal in the bootloader. I press connect and a pop up suggests /dev/ttyACM0 which I accept, another pop up ask me if i want to flash ArduPy, I click yes:
and then:
andrewh@punch:~$ /home/andrewh/.vscode/extensions/seeed.seeed-micropython-ide-0.0.6/tools/aip flash -o -p /dev/ttyACM0
/home/andrewh/.local/share/aip/ardupycore/Seeeduino/tools/bossac
ERROR: Exception:
Traceback (most recent call last):
File "pip/_internal/cli/base_command.py", line 186, in _main
File "aip/flash.py", line 140, in run
File "pip/_internal/operations/prepare.py", line 287, in unpack_url
File "pip/_internal/operations/prepare.py", line 159, in unpack_http_url
File "pip/_internal/operations/prepare.py", line 299, in _download_http_url
File "pip/_internal/network/download.py", line 189, in __call__
File "pip/_internal/network/download.py", line 157, in _http_get_download
File "pip/_vendor/requests/sessions.py", line 546, in get
File "pip/_internal/network/session.py", line 405, in request
File "pip/_vendor/requests/sessions.py", line 533, in request
File "pip/_vendor/requests/sessions.py", line 668, in send
File "pip/_vendor/requests/sessions.py", line 668, in <listcomp>
File "pip/_vendor/requests/sessions.py", line 247, in resolve_redirects
File "pip/_vendor/requests/sessions.py", line 646, in send
File "pip/_vendor/cachecontrol/adapter.py", line 53, in send
File "pip/_vendor/requests/adapters.py", line 416, in send
File "pip/_vendor/requests/adapters.py", line 228, in cert_verify
OSError: Could not find a suitable TLS CA certificate bundle, invalid path: /tmp/_MEIawrMbI/pip/_vendor/certifi/cacert.pem
Please advise ?
Regards,
Andrew