Wio Tracker 2G bricked?

By the way, this is the output when I try to flash a sketch.

This same environment works fine with another Wio Tracker I have



Sketch uses 10072 bytes (3%) of program storage space. Maximum is 262144 bytes.

Atmel SMART device 0x10010005 found

Device : ATSAMD21G18A

Chip ID : 10010005

Version : v2.0 [Arduino:XYZ] Apr 18 2017 09:45:16

Address : 8192

Pages : 3968

Page Size : 64 bytes

Total Size : 248KB

Planes : 1

Lock Regions : 16

Locked : none

Security : false

Boot Flash : true

BOD : true

BOR : true

Arduino : FAST_CHIP_ERASE

Arduino : FAST_MULTI_PAGE_WRITE

Arduino : CAN_CHECKSUM_MEMORY_BUFFER

Erase flash

done in 5.005 seconds



Write 10332 bytes to flash (162 pages)



[=========== ] 39% (64/162 pages)

SAM-BA operation failed

An error occurred while uploading the sketch