WIO Terminal Workbench 1

Changed the power unit to LiFePO4 6000 mA followed by a DC/DC step up 3.2v to 5 v and a charger module So I can charge the device with my phone adapter.
The PMS5003 needs 5v but data lines are 3v3 so no need for level shifter when connecting to the WIO terminal.

because I have only one , I made The WIO terminal ‘clickable’ on the project box :wink:

one step closer - SERCOM UART on grove port working :sweat_smile:


WIO connected to pms 5003 reading particle sensor data

next step : CO / CO2 / TEMP and HUM sensors , a nice screen and alarm settings menu (maybe data storage on SD card / LoRaWAN connection ?)


playing with I2C

idea : interfacing thermal receipt printer to WIO terminal
(needs external power source and bi directional level shifter)


new out of the box selftest … firmware from 2013 :upside_down_face:

RPI adapters have a little higher voltage output (5.3 V) then regular phone charge adapters and that’s good for this thermal printer.


under construction :yum:


Si7021 temp/hum sensor

easy way to connect some diy electronics to your WIO terminal with
this cheap Proto HAT Shield Extension Board for Raspberry Pi 3

I added myself a 40 p double row 90 degrees

is it possible to decode audio with this little I2S PCM5102 DAC Decoder ? :thinking:


not yet :sunglasses:


but imagine :rofl:

Nice :star_struck::ok_hand:, This looks cool :sparkles:


thermal printer interface… almost done

library used

wired or wireless (BT) :thinking:


idea : handheld AirQuality analyser / data logger
waiting for the SCD30 sensor

handheld enclosure
sensor Sensirion

’ This article describes four routines designed to make it easy to write games in C that use sprites on the Seeed Studio Wio Terminal. They allow you to plot erasable sprites, check sprites for collision, and move sprites on the screen while avoiding flicker. ’

getting BMP image on the terminal


WIO as a wireless LoRaWAN datamonitor

haven’t been active with LoRaWAN for a long time, lucky I saved a sensor and some gateways, put a fresh battery in it and it started working on the TTN network again :sweat_smile:

I Put it outside to check and the temp is dropping So the sensor works. Now I want that data on the WIO terminal (for fun and learning)
Because we are on COVID lockdown in the Netherlands lots of free time now :upside_down_face: to try this.


LoRaWAN temp/hum sensor

I have an MQTT broker running on my home network and I am preparing some nodes to measure airquality (indoor and outdoor) and display data on the WIO terminal when switched on.


wifi mqtt-broker (mosquitto) on RPI


some old LoRaWAN project nodes that I will use


replacing bootloader

Seems so good! Feel free to share with us more :smiley:


CO2 / temperature / humidity sensor arrived :slightly_smiling_face:


test I2C RFID EEPROM Breakout - need some work on library