A related query based on reivilo’s query. I would like to check of the Arduino drive is accessible from a program. I have no issues writing or reading from the program to either SD or FLASH. I can make the arduino drive visible on my system write files to it but if the wio is powered on or reset the file is deleted.
It would be good if the contents can be made visible to a program. Use case would be to replace the SD card with flash and write configuration files to flash for reading/writing by the program.