@Brian527 Arrrrrr, thanks guys, I’m not sure if I like the device or not, at this point I am so frustrated with it that I may just have to use a M5Stack. This looks like it has potential to be a really good product. But WiFi not working, and other issues that I’ve had is enough to make me put it in a box and never think about it again. I get the impression that I may not be alone in that thought from some of the posts, thou it seems like if the issues are worked out these really are great.
Thanks again, I’ll look into the multiwifi library you suggest Richard and see if that doesn’t solve my biggest issue.