I was able to do the updating etc and load the example wifi client sketch. It operates and Pulls data from a webpage. Alas it only does this 10 times before it generates and errno 12 “not enough space” message. I cannot find what is taking up the space. It fails even if I pull no data but make the connection to the webpage only. So it is somewhere in the connect/disconnect that resources are not being released.
Any Ideas?