I have followed the documentation to load the EdgeImpluse.uf2 firmware. After entering bootloader mode and dragging the uf2 file to the Arduino drive, Wio Terminal did reset and the Arduino drive appeared again. (I tried loading other firmware like “CircuitPython” without problem).
After the above step, I launched Edge Impluse Daemon but it could not connect to the Wio Terminal. I have checked that the COM port is correct:
Edge Impulse serial daemon v1.7.3
Endpoints:
Websocket: wss://remote-mgmt.edgeimpulse.com
API: https://studio.edgeimpulse.com/v1
Ingestion: https://ingestion.edgeimpulse.com
? Which device do you want to connect to? COM10 (Microsoft)
[SER] Connecting to COM10
[SER] Serial is connected, trying to read config…
[SER] Failed to get info off device Timeout
[SER] Serial is connected, trying to read config…
[SER] Failed to get info off device Timeout
[SER] Serial is connected, trying to read config…
[SER] Failed to get info off device Timeout
[SER] Serial is connected, trying to read config…