This is what im getting in the error mesage.
Ive installed all the libraries and can compile and run my own code, really want to see if this will work. The monitor raspberry Pi program works great, just not this
Arduino: 1.8.12 (Windows 10), Board: “Seeeduino Wio Terminal, Enabled, 120 MHz (standard), Small (-Os) (standard), 50 MHz (standard), Arduino, Off”
In file included from c:\users\drew\appdata\local\arduino15\packages\seeeduino\tools\arm-none-eabi-gcc\7-2017q4\arm-none-eabi\include\c++\7.2.1\list:60:0,
from C:\Users\Drew\Documents\Arduino\libraries\Seeed_Arduino_Linechart-master/seeed_graphics_define.h:26,
from C:\Users\Drew\Documents\Arduino\libraries\Seeed_Arduino_Linechart-master/seeed_graphics_base.h:2,
from C:\Users\Drew\Documents\Arduino\libraries\Seeed_Arduino_Linechart-master/seeed_line_chart.h:2,
from D:\Documents\Seeed Stuff\AcceleratorReadings.ino\AcceleratorReadings\AcceleratorReadings.ino:2:
c:\users\drew\appdata\local\arduino15\packages\seeeduino\tools\arm-none-eabi-gcc\7-2017q4\arm-none-eabi\include\c++\7.2.1\bits\stl_algobase.h:243:56: error: macro “min” passed 3 arguments, but takes just 2
min(const _Tp& __a, const _Tp& __b, _Compare __comp)
^
exit status 1
Error compiling for board Seeeduino Wio Terminal.
This report would have more information with
“Show verbose output during compilation”
option enabled in File -> Preferences.