Wio Terminal -- Can't Erase the Initial Wi-Fi Factory Firmware

I am using the Mac OS 13.5.2, trying to erase the initial Wi-Fi factory firmware, and I’ve also slid the power switch twice quickly, but no matter how hard I’ve tried, it still doesn’t work.

After I typed the command python3 ambd_flash_tool.py erase in terminal, I’ve got this error log below.

Set binary mode
version()=1.1 [Arduino:XYZ] Mar 12 2020 17:43:33
Connected at 921600 baud

SAM-BA operation failed
wait...
wait...
wait...
Flashing...
error: Enter Uart Download Mode
Image tool closed!

Error!

Thanks for any help.

Perhaps you can try to connect to the computer with another cable that can carry data

Here is also a solution for the error: Enter Uart Download Mode message.

Thanks a lot for your kindly help, it truly worked. :smiley: