I’ve spent an… interesting… day at:
https://wiki.seeedstudio.com/Wio-Terminal-Network-Overview/
… trying to set my Wio Terminal up as a webserver.
Early on, we are told to update the Wi-Fi core of the RTL8720 before usage… and given a small sketch to check what version our core is after we try to do that.
But no indication I could find of what version number we should see when we do the check. Can anyone help?
I’ve got the sample code running… but it takes a long time… 10-30 seconds it seems like… to get past the “WiFi.begin”, and then it never leaves the “while (WiFi.status() != WL_CONNECTED)” loop.
Ideas? (And yes, I’m using Seeed_Arduino_mbedtls-dev)
All this using a Windows 10 PC.
(I’ve successfully set up webservers in other Arduinos before.)
===
I’ve been successful with the simpler “Scanning Wi-Fi Network Example Code”.
NOT successful with “Connecting to Specified Network Example Code”. (Fails the way the webserver code fails. And yes, I did put my ssid and password in, and AP is broadcasting the ssid. 2.4GHz WPA-2 Personal. (Arris Surfboard… Firewall set to medium. Reducing to “low” didn’t help.)