Wio Terminal - Arduino Serial Communication

@Citric I specified Serial1 for the Wio Terminal.

It works when I send from the Wio Terminal and receive from the Arduino.

But when I send from the Arduino Uno and receive from the Wio Terminal, the code doesn’t work, I don’t see the “Hello” string received in the Wio Terminal’s Serial Monitor.

// Sender - Arduino Uno
char mystr[6] = "Hello"; //String data

void setup() {
  // Begin the Serial at 9600 Baud
  Serial.begin(9600);
}

void loop() {
  Serial.write(mystr,6); //Write the serial data
  delay(1000);
}
// Reciever - Wio Terminal
char mystr[10]; //Initialized variable to store recieved data

void setup() {
  // Begin the Serial at 9600 Baud
  Serial1.begin(9600);
}

void loop() {
  Serial1.readBytes(mystr,6); //Read the serial data and store in var
  Serial1.println(mystr); //Print data on Serial Monitor
}