Hello, first post so not sure if I’m in the right place. I’m looking at getting the Wio Terminal with the LoRa/GPS expansion pack but I have questions. Firstly is there a working version of meshtastic available for it? I’ve searched high and low but haven’t found any definitive answers or links
secondly I’m also looking at the battery expansion too, what’s the average run time with LoRa active and has anyone upgraded the 650mah battery to something a bit higher? Any information is greatly appreciated thanks
Welcome… I do not have this device but hopefully someone on here may be able to help… you are in the right place!
Ah thank you! Well fingers crossed, I am looking at ordering one next week so I’d like some info in advance before I make a final decision:)
i dont know what time zone you are in… but the Seeed guys dont come to work for another 8 or 9 hours
I’m in the UK, I’m in no rush though, plenty of time until I make a decision haha
Hi @Alan_Ball the Wio terminal is not yet support Meshtastic yet.
but we will add a LoRa expansion board for XIAO ESP32 and nRF52840, so that will make XIAO a meshtastic-enabled dev kit.
Stay tuned
2 Likes
Ah I see, well thanks for the feedback ![]()
1 Like