WIO Terminal analog inputs 5V or 3V3?

The power output voltage of the Grove interface is 3.3V. If you have the need to use 5V, you can choose to connect to the 5V supply on the back of the Wio Terminal.

1 Like