Wio-Terminal 650mA battery - Red LED

I wanted the ability to leave the 650mA battery on at all times and to utilize the low power modes from the Wio-Terminal CPU. The red LED on the battery module would be a waste of power for my projects, and i was wondering if there is a way to disable it through code.

If the LED can’t be disabled through code, would there be any adverse effects if I removed the LED from the board or cut the trace?

EDIT: It seems that that Yellow LED is also on during normal operation, so my question also applies to that.

Thanks,

Richard

Hi @richard.seguin,

Please check the schematics for the battery chassis below.

https://files.seeedstudio.com/wiki/Wio-Terminal-Battery-Chassis/res/WioTerminal_battry_650mAh.rar

It seems that the LEDs are not directly connected to the pins of SAMD51 and therefore you cannot turn them off using code.

I highly doubt that cutting the traces would make an impact on power saving, because these LEDs draw very little current.

And also, it’s not a very safe procedure to cut the traces physically.

Best Regards,
Lakshantha

I agree with Richard. That was a big mistake to not allow turning off the led on the battery. Who want’s to use a tiny pin to turn off the battery any time the unit is not used for a while. Hopefully on a future model of the battery you guys will think about the practicality of actually using this thing. Why would you have an led to show you are discharging the battery, when the LED itself is what is discharging the battery ?