Seedstudio makes a rubber case for their SARK-110 Antenna Analyzer that looks like it might fit the DSO Quad/DS203 . Path=63_65. Looks like the SARK-110 is built on the same case/chassis as a DSO. Has anyone tried this out? I don’t own a DSO Quad yet but am definitely going to be purchasing one soon and being that I plan on using it in an automotive garage environment, a protective case would be great. On a side note, great forum, lots of good info here, glad I found it.[size=1]whatsapp web 192.168.0.1 routerlogin
[/size]
Hi.
The SARK-110 Protective Rubber Case dimension is 110mm x70mm x16mm and DSO Quad - 4 Channel Digital Storage Oscilloscope Dimension is 98 * 60 * 14.5 and button placemnet is little bit different.