Hi Seeed_Harrison
Is there any way to disconnect the power from the Seeed XIAO RP2040 USB connector when the device is connected to a USB port?
I need to have power from USB, but if USB power is disconnected then I need fail safe power fall back to be from the external power source.
Would I need to have another usb connector with a circuit to select the power source, which then connects to the Seeed XIAO RP2040 usb connector?
Sort of like a pass through like this hdmi pass through?
Thank you.