Hi,
Will connecting the +5V and GND pins on the Seeed XIAO RP2040 to an active external power source cause any problems if the USB C is connected simultaneously?
Thank you.
Hi,
Will connecting the +5V and GND pins on the Seeed XIAO RP2040 to an active external power source cause any problems if the USB C is connected simultaneously?
Thank you.
Hi there, and welcome here…
Did you read the wiki and the power pins if its not spelled out on the rp2040 like on the other xiao’s not sure why . Anyway a diode is needed between 5V external source and the pin as to not harm the xiao.
Check some of the other threads as well on it.
HTH
GL
PJ ![]()
from the Xiao Esp32S3 for example:
I do see a caution on the rp2040 Wiki about having both, so read the manual.
and here in the online schematic I do see a diode between Vin and VBUS so there’s that
Hi,
Please don’t do so. As mentioned on its wiki page:
For power supply pins: The built-in DC-DC converter circuit able to change 5V voltage into 3.3V allows to power the device with a 5V supply via VIN-PIN and 5V-PIN.
XIAO RP2040 currently only supports battery power supply and cannot connect to Type-C while a battery is connected, as it may pose a safety risk.
Please use one kind of power supplying method at a time (USB-C, 5V pin, battery connected to VIN pin).
Hi Seeed_Harrison
Is there any way to disconnect the power from the Seeed XIAO RP2040 USB connector when the device is connected to a USB port?
I need to have power from USB, but if USB power is disconnected then I need fail safe power fall back to be from the external power source.
Would I need to have another usb connector with a circuit to select the power source, which then connects to the Seeed XIAO RP2040 usb connector?
Sort of like a pass through like this hdmi pass through?
Thank you.
Yes, a power managing system is needed for your intent. But I think a better solution is to use another XIAO with charging PMIC. Please check the comparison table here: