Hi all i’ve read the WiFlyGSX-um2.pdf and i have an Wifi Shield.
For activate the ad hoc network this document write :
To enable adhoc mode via hardware set PIO9 high (3.3V) at power up. On the RN-134 PIO9 is on the J1
jumper block. When the module powers up with PIO9 set high, the WiFly module creates an adhoc
network with the following
SSID: WiFly-GSX-XX where XX is the final two bytes of the devices MAC address
Channel: 1
DHCP: OFF
IP address: 169.254.1.1
Netmask: 255.255.0.0
And in the shield … where is the j1 jumper ?