WiFi Bee Programming

Hello,
I have a WiFi Bee Standalone Module with atmega328 onboard.
My Problem is that I cannot connect to the board via serial connection.
I’ve also tried to program the ATmega828 straight from the Arduino IDE but that also wasn’t successful.
The module is not responding at all. I’ve put the module into the grove header board but also not successful.
What can I do to get this thing working? I was thinking of soldering an ISP header to the board and program it directly with an ISP programmer but that is my last option which I do not want to choose at all.

Any help would be great.

Thanks in advance.

  • ftrueck -